This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31520: About 1Vout efficiency curve of LMZ31520

Guru 19645 points
Part Number: LMZ31520

Is there efficiency data of below condition for LMZ31520?

⇒PVIN:3.3V、VIN:5V、Vout:1V、Iout:~20A

※Datasheet is described only PVIN:3.3V、VIN:5V、1.8Vout.

    Webench can't simulate PVIN:3.3V condition.

Best regards,

Satoshi