I've designed a rear lamp for a car for the EU market, with stop, tail, and direction indicator functions. There are two LM3429s on the board, one for the stop, and one for the directin indicator. Both are operating in boost mode. The two circuits are very similar, differing only in a few resistor values, since the direction indicator string runs a 200mA, and the stop light runs at 110mA. They are permanently powered, but held off by holding the nDIM pin low (<0.5V) when the light is not required. They work perfectly when the light is on (nDIM >4.5V), but when in the off state, the direction indicator circuit runs hot - I'm guessing at least 50°C as it's too hot to touch for more than a second or two. I can't see any great differences between the voltages on the hot circuit and those on the cold circuit, nor can I explain what might be causing the excessive heat output. Any ideas?