This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62400-Q1: TPS62400-Q1 Cff

Genius 4840 points
Part Number: TPS62400-Q1
Other Parts Discussed in Thread: TPS62400

Our customer consider to use TPS62400.

They would like to use following FB resistor value.

VIN=3.3V

Vout1=2.8V

Iout1 max =0.3A

R11=54.9kΩ

R12=15kΩ

Cff1=

 

Vout2=1.8V

Iout2 max =0.3A

R21=30kΩ

R22=15kΩ

Cff2=

In this case,they need Cff capacitor,if you recommend value,please let us know it