Other Parts Discussed in Thread: BQ40Z50-R1
Dear support,
as i understand bq20z655-r1 can perform standalone, therefore I'm considering it for our new Battery Pack project.
Unfortunately (according to datasheet page 16, "SBS Commands" table) maximum current is 32A, and capacity 65Ah.
I need more than 300Ah capacity and 300A discharge current.
In datasheet (page 20) application schematic, 10mOhm shunt rezistor is used.
Let say i change shunt resistor to 1mOhm and make the bq20z655-r1 think that 1A current flows (while actual current is 10A), capacity should go up 10 times.
The question is: will State of charge calculation algorythm perform properly if bq20z655-r1 sees 10 times lower current than actually is.