This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59208F: I2C and Power dissipation

Part Number: TLC59208F

Hi,

http://www.ti.com/lit/ds/symlink/tlc59208f.pdf

1- I tried to calculate the power dissipation of the TCL59208F when driving several LEDs. I'm missing somes informations like the Switching MOSFET's Dissipation, PWM consumption. In my calculation, I have included the supply current, maximal current per ouput (around 40mA for 4 channel), and a low SDA (30mA @Vcc 5V). Is it close enough ?

2- Low level output current is 30mA max on the recommended operating condition p 5/37. A bit further, the same low level output current is mentionned at 30mA min. What current should I used to the calculate the pull-up SDA resistor ?

Thanks,