Other Parts Discussed in Thread: BQ27531EVM, , BQSTUDIO
Hi,
I am doing development work on BQ27531EVM demo board (Bq27531-g1 gauge and bq24192 charger). The battery that I'm using is Panasonic NCR18500A (1900mah).
While I'm doing the learning cycle, I observed that the charging current is only around 0.463A. I'm using USB charger connected to laptop with PSEL and OTG set to HI which will make INLIM set to 500mA limit. I want to increase the charging current to its 1.38A standard rating but I can't seem to do this.
I also tried to charge the battery using power supply connected across VBUS and GND (6V, 3A) and changed the PSEL to LOW. The INLIM bits changed to indicate 3A current limit, but the charging current never increased. How can I increase the charging current, then?
Also, you mentioned and I also read in the datasheet that the default charge current must be 2048mA for this part. But when I read Reg2 [ICHG[5:0]], the value is 1'b011000. How does this equate to charge current in mA? What does this value mean? I'm pretty sure it's not 2048mA because my measured charging current is only around 0.463A. I also see that there is no way for me to change these bits as it is controlled by FG's algorithm. Is my understanding correct?
This is my first time to work on batt gauge and charger ICs so Any input is appreciated
Thansk!!