This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A49: is R1 in the Datasheet's (Rev. E) Detailed Design Procedure (Section 9.2.2) wrong?

Part Number: TPS7A49


Hello team,

I was going through TPS7A49's Datasheet and in Section 9.2.2 where the "Detailed Design Procedure" example is described, R1 is calculated to be 1.265 kΩ in Equation (5), however the result is followed by this statement: "For R1, select a standard, 1%, 68.1-kΩ resistor".

It seems like a 68.1 kΩ resistor would set the output to 2.0 V instead of 1.2 V—could you confirm this is a mistake and that R1 should be 1.27 kΩ as the closest standard 1% resistor value?

Best Regards,
Victor