Hi,
Pls. provide the Max current needed for the TPS65133 Inductors.
In the DS I didn't find this information and the recommended parts have very high current and they are too big for me.
I need to optimize this part
Regard
Zeev Gerber
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Pls. provide the Max current needed for the TPS65133 Inductors.
In the DS I didn't find this information and the recommended parts have very high current and they are too big for me.
I need to optimize this part
Regard
Zeev Gerber
Since I doubt may users will frequent this forum on Christmas, I will answer this. The peak inductor current during normal operation is Ipk = (Iout / (1 - D)) + (ILp-p / 2). TPS65133 specifies the current limit as valley current, so the peak current at current limit is Ipk = IOCL + ILp-p. I typically design my circuits with inductors rated to handle the peak current at current limit. This does result in a larger physical inductor, but a direct benefit is higher current rating = lower DCR = better efficiency. If you want to use a smaller inductor, that is up to you. It will be fine in normal operation, but may saturate or overheat under fault conditions. Calculate you maximum switch current in your application and choose an inductor that meets that rating.
Hello Zeev,
Please have a look in this app note for the boost converter calculations:
In addition, please check the current in the inductor during startup of the output voltages. During startup, most probable the inductor current is higher than during normal operation because the output capacitors need to be charged.
Best regards,
Brigitte