Hi,
My customer have a question.
Q.
In Table 2 of datasheet P17, C6 (C8 is a typo?) Is 100pF.
Why is it different from the result calculated from Equation (14) (16)?
Best Regards,
-watanabe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Table 8 C8=100pF for 12V out is correct and this was bench verified. As for the equation (14) calculate the crossover frequency, it is just simple estimation, always have some difference compared with the test, as for the equation (16), configure the zero introduced by CFF close to crossover frequency, it is normal design guideline.