This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3613-01: TPS3613 current consumption from VBAT

Part Number: TPS3613-01

Hi

I am planing to use TPS3613 in a board with VDD 1.8V 

On this board TPS3613 VOUT is connected to an SRAM device that requires 0.5uA in standby mode

my question is what is the maximum current that TPS3613 consumes from VBAT excluding the 0.5uA it drives the VOUT (IOUT)TPS3613_Sch.pdf

attached relevant schema