I am using a TPS62160 to supply 3.0 Vcc to a MCU with very little current. The system have work pretty well until I try to use a Lead-Acid Battery. I have follow all the datasheet recommendation, and for any other source of power (regulated power supply, alkaline batteries, USB) it works perfectly. But when I try to use a Lead-Acid battery, the component, and also my MCU burns immediately.
The datasheet say this about "Power Supply Recommendation" :
"The TPS6216x device family has no special requirements for its input power supply. The input power supply' s
output current needs to be rated according to the supply voltage, output voltage, and output current of the
TPS6216x."
Since all of these is checked, I have no idea about what is the problem.
I'd really appreciate any help or suggestion :)