Hello,
I am considering using this controller IC UC28023, but I need to be able to drive a synchronization clock to the device. In the electrical characteristics section it specifies it only as an output pin.
In another section it says that the clock pins can be tied together on two close devices, implying that the pin is not just an output.
I was wondering if I could get some clarity on the Clock pin characteristics, as to whether it can actually be an input as well, and if so, what are those characteristics?