I have used BQ76PL536A-Q1 IC for monitoring two sets of 6 cell batteries. In one of the systems, the cell number 4 was gradually discharged by BQ76PL536A-Q1 and the cell voltage reach to 0.6v and cell number 4 break down.
In the second IC, after a one day of work in 45 degree temperature, the voltage of first cell was displayed as 1.5 V while that of the fourth cell was 5V. However when measuring with a multimeter, both cells voltage were equal to 3.3V. why?