This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61225: Short-circuit when powered from a CR2032 coin-cell battery

Part Number: TLV61225

Hello,

I am powering my board using the TLV61225 boost IC with a CR2032 coin-cell battery (nominal voltage 3V when fully charged) to output 3.3V

The circuit draws about 20 mA under load (only 2 LEDs are powered up at a time). According to fig 1 of the datasheet, the boost should be able to source at least 160 mA

When powered from a coin-cell, the circuit draws the maximum amount of current the battery can provide and discharges it in seconds. Seems like a weird mode where the boost is short-circuiting the output.

When powered from a bench power supply with a fairly high current limit (~ 200 mA) the circuit works perfectly and the regulation looks OK (at light load and under load). However lowering the current limit of the bench supply to around ~ 100 mA recreates the behavior of the coin-cell : short-circuit, the boost draws the maximum amount of current. 

Here's my schematic (R11 is not loaded):

What explains this behavior and how to fix it?

Thanks for your help!

  • could you help to measure the VIN, SW and VOUT waveform of the "short circuit" behavior you observed?
    as the input power is limited, coil cell or 100mA power supply, the boost converter start up behavior and the maximum load power are matter.
    avoid applying load during the boost converter startup. and make sure the peak load power is lower than the input source capability.