Part Number: LM2776
LM2776 data sheet suggest: "In typical high-current applications, TI recommends 0.47-μF or 1-μF 10 V low-ESR ceramic capacitors for the
flying capacitors".
What is "typical high-current" value referred in the data sheet for TI recommended flying capacitor value?
My customer is using 0.1-uF flying capacitor & want to know, if 0.1-uF can be used for < 20mA load?
With 1-uF capacitor LM2776 output voltage is doesn't increase beyond -1V for 3.3V input. Output increases to -2.7V with 0.1-uF with 3.3V input.