This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24296: NOT Coming Out Of Boost Mode

Part Number: BQ24296

Dear,

1)I am using this ic in one of my project.I am also able to start the boost mode,at the time of boost mode PMID voltage 5,Vbus voltage 5 and Vsys voltage 3.98.

Register value before activating the boost mode:-

REG00=0x37, REG01= 0x1B,REG02 = 0x3C,REG03= 0x11,REG04=0xB3,REG05= 0x8A,REG06=0x73,REG07= 0x4B;

Register value when  boost mode activated:-

REG00=0x37, REG01= 0x2B,REG02 = 0x3C,REG03= 0x11,REG04=0xB3,REG05= 0x8A,REG06=0x73,REG07= 0x4B;

In boost mode,when i reconnect input supply 5v to Vbus,the PG_STAT doesn't change. The internal REG08[2] didn't set(1 – Power Good) automatically.Even no Interrupt generated at that time.

Can u suggest,how to overcome this problem.?

2)I also changed the boost mode voltage at 4.55(offset voltage),at that point problem is same?

Thank you in advance.