This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23861: About TPS23861 I2C Isolated Question

Part Number: TPS23861
Other Parts Discussed in Thread: ISO1540, ISO1541

Hi Sir,

Our system only have single I2C data line, how to connect to TPS23861 with isolator?
I can use ISO1540 to implement?

  • Hi Wenyung,


    As long as the isolator is bidirectional, the SDAI and SDAO can be tied together. Please refer to the schematic of the 6kv lightning surge board I sent you. ISO1541 is used in that board(ISO 1541 is very similar with ISO1540).

    Best regards,

    Penny