I have a customer who is using the LM5033 as an isolated bus converter in a design and will be using the REF pin similar to as shown in the application note. It says in the datasheet however that the minimum current sink is 5mA. Does this imply that they need to size the pull-up resistor to accommodate this minimum current? I noticed that Figure 8 in the datasheet shows good reference all the way down to 0mA and the app notes have a relatively large pull-up resistor, 20kohms. If lower current is ok, why does the datasheet have a minimum value? Another similar question was asked in the thread below. If Iref is between 0-5mA, why isn't Vref pulled down?
Thank you very much!
Russell