Hi,
One of our customer is now using TPS65217C. They have met a problem now that when the AC pin (from AC/DC adapter)voltage drop from 5V to under 3.2V, then re-connect a 5V input voltage to AC pin, the device has no output voltages both on LDO and DCDC. Only the INT_LDO and BYPASS pin voltage is normal, RESET(44PIN)voltage is 3.5V,Pin PB_IN is floating and the voltage is low level.
Could you kindly help to check this?