I am using BQ21040 part for charging Li-Ion battery with following hardware specification.
Input capacitor: 1uF/16V ceramic X7R, 10% tolerance
Output capacitor: 1uF/16V ceramic X7R, 10% tolerance
RISET: 1.2K ( corrosponding to 450mA)
RTS: 10K, as i am not using NTC feature of it.
Pulled up CHG pin with 10K.
but practically seeing the charging current of the battery is 214mA, which should be 450mA for 1.2K resistor.
please help me in resolving the issue.
Regards
Manish