Part Number: UC3841
Please provide download link of the application note mentioned in the datasheet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Arumugam,
The schematic references and old Unitrode application note U-114. I tried to see if I could find this first through TI’s web site and then google. I happened to have an old Unitrode application book from 1997. This application book does not even have this application note. The publications go from U-113 to U-115 skipping U-114. I have never seen this application note and also do not believe it is available.
I went to the TI reference design center to see if I could find UCC2/3841 offline 15V power converters. I did not find a reference design using the UCC2/3841 however, I found the following reference designs with the following outputs. http://www.ti.com/general/docs/refdesignsearchresults.tsp Maybe one of these will work in your application.
Regards,
Mike