Other Parts Discussed in Thread: TPS3820
Hi, team,
My customer met one question about TPS3820-50-Q1.
They use a switch to control the WDI and MCU connection, when in programming the switch is OFF, when in normal work the switch is ON. Thus when in programming, TPS3820 will not reset MCU.
They are concern about the noise in Automotive system, so they do not like WDI pin to be floating, and a 100k resistor is added from WDI to GND by the device.
I checked the TPS3820-50-Q1 block diagram, if WDI is floating, internal Auto-reset oscillator will generate signal to transition detector through a 40k resistor.
My question is as below.
1. Is customer's 100k pull-down resistor connection ok if WDI is not floating?
2. What is the output voltage of Auto-reset oscillator? What is the voltage threshold of Transition detector?
3. Customer tested that if the WDI-GND resistor is >36k and Switch OFF, TPS3820-50-Q1 will not output reset signal. This should be related with the WDI pin voltage.
4. About the 100k resistor to GND, could you give more comments about the other risk to system?
Thanks.
Johnny