I had a couple questions regarding a TI buck/boost converter. I recently had a couple PCB panels made and I’ve run into a bit of an issue with sourcing the right sized parts. I made the mistake of assuming that I would be able to find all of my components in a 0201 (imperial) package size and I’m unable to find two inductors and a capacitor. The design I’ve implemented uses a TI TPS61090 “Synchronous Boost Converter” to regulate my voltage for my system. Here are my questions:
1. When I do the calculations for the L1 inductor (assuming Vout is 3.3V, Vbat is 2.75V, and a maximum output current of 500mA), I get a value of ~5uH. The largest inductance I can find in a 0201 package size is ~270nH. My understanding is that the input inductor helps minimize “ringing.” What would be the ramification of using an inductor that much lower than the calculated value? Why does the required inductance increase as the maximum potential current decreases? Would it be more ideal to go this route, or to solder super small wires onto the board and have a larger inductor (that won’t fit on my pads) floating in free space?
2. My second question is essentially the same but for the output capacitor. With my calculations (same parameters and ripple of 10mV) I get a value of ~14uF. The largest capacitor I can find in a 0201 package size is ~10uF. However, the note suggests that the capacitor I use should be almost double the calculation due to load transients. Also, it appears the capacitor should be polarized. How necessary is it for the capacitor to match? What will the effect be if it is off by a bit? Does it have to be polarized or can it be unpolarized (unpolarized would be ideal)?
Thanks.