This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62565: About Inserting Resistor of Between VIN to EN.

Part Number: TLV62565
Other Parts Discussed in Thread: TLV62568

Hi,

My customer wants Inserting 1kohm Resistor of Between VIN to EN.

Is this all right?

Could you tell me if limit current of EN.

Best regards,

Watanabe

  • Yes, a resistor of that low a value is ok but unnecessary. The EN pin is an input, which draws a leakage current which is shown in the D/S.

    As well, please use the newer TLV62568/9 instead of the TLV62565. They are pin to pin and more efficient.