This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

125 C Ta buck needed

Guru 29720 points

Other Parts Discussed in Thread: TPS54362-HT, TPS62000-HT

Hi Team,

Is there any device that can operate under the following condition?
--------------------------------------
・Vin: 5.4V
・Vout: 2.6V
・output load: 0.35A(MAX)
・fsw: 3MHz
・Ta: 125℃
--------------------------------------
I would like to confirm if my customer should select DCDC controller in this case.

Best Regards,
Yaita / Japan disty