This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61194-Q1: Boost Start time is 0.5ms instead of 50ms

Part Number: TPS61194-Q1
Other Parts Discussed in Thread: TPS61194,

When I enable power to my TPS61194, and enable (pin 4) is set to 3V3, the BOOST converter starts in 0.5ms instead of the 50ms claimed in the data sheet, Figure 18.

In the figure below,

Channel 1 is the input power, 12V. 

Channel 2 is the boost converter output.

There is a delay of approximately 65ms from applying power to the converter starting. This is the device soft start time. There should then be a 50ms window where the boost converter starts up. In the figure below, the boost converter starts in approximately 0.5ms. This causes an inrush current large enough to trip our load switch and so the input voltage is turned off. I have tested this on an eval card and the eval card behaves the same. Can somebody tell my why I do not have a boost start time of 50ms

Thanks