I am working with a system that uses an off the shelf charger and 5-cell, 4Ah LiPo battery packs. The charger has protection and balancing built in, but the battery packs do not. I'm designing a motor control system that uses these battery packs: http://www.batteryspace.com/powerizer-polymer-li-ion-battery-18-5v-4ah-74wh-30c-w-o-pcb-for-rc-flight----ce-listed-un38-3-passed-ndgr.aspx
I need a gas gauge and protection for the battery during discharging. I looked at the BQ76920, BQ78350 combination for this, but I think it is overkill for my application since I do not require balancing or charge control. I am a bit confused by the other offerings TI has, and I am wondering if there is a more appropriate IC for this application.
Also, I need some communication back to the MCU indicating faults, charge level, etc.