Other Parts Discussed in Thread: OP27
Hello,
I am working on building a constant current DC power supply. It consists of two full H-bridge DC-DC converters feeding two HF transformers. The secondary side of HF transformers are connected with diodes and outputs are paralleled to provide total output current. I'm using two UC2846 peak current mode control IC to regulate the power supply output. I'm facing problem when paralleling two PWM ICs, one of the PWM IC outputs (Aout, Bout) goes low. The control configuration is shown in image below. (IGBT-1,2,3,4 are IGBT modules that contains two devices in them, high side and low side. IGBT-1,2 are for Inverter-1. IGBT-3,4 are for Inverter-2) The following points are significant in the design.
1) Shutdown feature is not used (Pin 16 is connected permanently to GND)
2) Timing capacitor pin (Pin 8) in slave PWM IC is connected to GND.
3) Sync pin (Pin 10) of both master and slave PWM IC are connected together.
4) Error amplifier in UC2846 is used in unity gain configuration ( Pins 6 and 7 are shorted) in both master and slave PWM ICs.
5) Identical slope compensation is used for master and slave PWM ICs (Ramp waveform available in CT pin of master is used for slope compensation in slave)
6) External analog PI using OP27 op-amp is used instead of using E/A+, E/A-, Comp pins to construct PI as suggested by datasheet.
The design works fine with single H-bridge inverter but when two inverters are operated in parallel one of the inverter PWM pulses goes low.
I have two questions.
1) I would like to know if the way two PWM ICs are paralleled is correct? or Is there any other way to parallel.
2) Connecting two Sync pins to have a unified clock reference is sufficient or any external circuit is recommended to connect two Sync pins?
Any answers / suggestions?
I'm curious to know about using this UC2846 PWM IC to parallel two full H-bridges. So kindly avoid suggesting to change power topology or of that sort!
Thanks,
Mervin.