Other Parts Discussed in Thread: BQSTUDIO, EV2400
About the BQ27421-G1A, as we know, the procedures for the generation of golden image (*.gm.fs) are listed as follows:
1) The procedures for the generation of golden image (*.gm.fs) based on the calibration result (*.gg file)
1-1) Connect the device with EV2400. And then, run the bqStudio.
1-2) In the bqStudio
1-2-1) Click the "Data Memory", and click "Import" button to import the *.gg.csv file.
1-2-2) In the "Preferences", in the "Golden Image", clear the "Class Names to be Preserved in GMFS Files" field to be empty.
1-2-3) Click "Write All" ,and then, wait couple seconds.
1-2-4) Click "Read All" ,and then, wait couple seconds.
1-2-5) Click "Golden Image" button and press "Create Image Files" button.
1-2-6) Then, the golden image (*.gm.fs) is generated in the local drive.
Are the procedures above correct?
Thank you.