We have been following the learning cycle as described in a previous post. We are able to fully charge our pack and the OCVTAKEN flag is set at which point we start the discharge cycle. This is where we have tried a couple of different things without success:
We fully discharged the batteries ~600 mV below the 'Cell Terminate Voltage'
- at a rate of C/20 (as suggested by this post) AND
- at a C/8 rate as suggested by the initial post
We waited until the OCVTAKEN updated but neither QMax updates nor Learned Status changes to 0x05.
Is there something we may have set incorrectly that could prevent this update? We do have a leakage current that we can't control as it is an always ON device (battery is the backup source), could this be the issue?
I've gone through a few of the posts and tried a few other things without success. Any advice would be appreciated, logs for the latest discharge, charge, discharge cycles are attached.