Hello all,
I am using the Phase-Shift PWM Controller UCC2895 for a DC/DC full bridge ZVS converter of 6kW with a fixed frequency of 50 kHz.
Vin=400V and Vout= 100V to 400V
When I increased the output power, the primary current show an unbalanced wave form.
I am using gate drive transformer like in sluu421.
I improved with a better compensation loop but I still have the problem.
At the end the transformer is saturated!!! (On the picture the transformer is begining to sature)
Have you got a idea of what I have to modify to solve this issue?
Thanks in advance,
Best Regards,
Pierrot