Hello
Please adivse about TPS62510 for customer's New disign .
~~~~~
*Customer's spesificaiton
:Vin_min=1.5V~1.8V Vin_max=3.3V
:Vout=1.15V Iout_max=1.0A or 1.5A [
:Audio Application ( fPWM)
~~~~
I think Vin min=1.5V of this requiremtn is difficult , but I think TPS62510 seems suitable if Vin min> 1.8V.
However, TPS62510 has no Webench simulation support. and SwitcherPro also.
Also, I have no Pspice simulator.
I will buy EVM, but Would you please advise?
These are question( iquiry) from customer in advance to choose TPS62510.
Q1)
In case Vin=1.8V, Io=1A ( Vout=1.15V ) can be kept?
If available, in case Vin=1.8V, would you please have us characteristic curve like Fig 13 ? ( Fig 13 has Vin=1.9V, but no curve of Vin=1.8V)
Q2)
If available, would you please give us charactristic curve which is Vin versus Iout at Vo=1.2V if you have.
Best Regardas