Hello,
we are using the LM3150MH for the power supply of a small single board computer.
The design is rated 24 V (20-28 V) input to 5 V / 2 A output and was calculated using Webench.
Last year we produced several hundreds of this unit. Each unit was tested prior to shipment to
our customer. Now we got several boards back with defect power supply, and they all share the same
symptoms: The external high-side FET (CSD18504) has a short, and so connects the 24 V input voltage
directly to the regulators output - which causes excessive damage at the connected IPC board.
All these units worked fine first, but then failed after many hours or days of operation - some suddenly
during operation, others at turn-on.
I didn't check yet if only the FET has died or if the controller chip also is defect now, to not delay this post. We are urgently looking for the cause of these failures, and hope that someone can help us with the analysis. I am attaching the schematic circuit and a pcb view from CAD that shows both layers and the components.![]()
Many thanks in advance and best regards, Tilmann Reh