Part Number: CSD18540Q5B
A brief description about my application, controlling a 40V 15A LED load, 450W with PWM from microcontroller 0-5V. The power supply has capability of 500W.
Earlier I had built a circuit to control up to 200W with the power supply, using PWM and it worked fine. When I tried controlling the 450W, the mosfet didn't give out full output. So, I had to add a gate driver and external 12V supply to completely saturate the mosfet to 10V and worked fine, but had lot of fluctuations in between. Right now, i'm reconsidering the mosfet options, and if possible gate driver options. Any help in finding me the correct MOSFET would be highly appreciated.
Under the power mosfet section, we have three options, N-channel, P-channel, Power Mosfet module. [--Eliminating the P-channel Mosfets.]
I have come across CSD18540Q5B as best suited for my need.
Couple of questions for the experts:
1. Would the Mosfet run 40V 15A if the gate voltage is 5V, or does it have to be around 10V?
2. If the gate requires 10V, please suggest a good gate driver.
3. Any additional knowledge about my load connections or circuit connections would be appreciated.
Currently learning more about Power stage module under power mosfet, if you could suggest anything in this, as it has in built gate driver. that would be good.
Thank you
-Summi