Part Number: TPS62132
Other Parts Discussed in Thread: TPS62130EVM-505, TPS62140EVM-505, TPS62150EVM-505,
Hi, I'm creating my custom PCB using the TPS62132RGTR.
In the SLVU437A (TPS62130EVM-505, TPS62140EVM-505, and TPS62150EVM-505 Evaluation Modules),
the EVM used a shielded inductor XFL4020-222MEC.

The shielded inductors are quite expensive and big, compared to the 1008 inched unshielded inductors like the below one.

So my question is, do I really have to use the shielded inductor recommended in the EVM datasheet?
Or can I choose the unshielded inductor?