Hi, All
In GPC tool calculation, there are some files required. I use the EVM (bq27541) to log data. There are some data to log, But there is no clear requirement in GPC implementation guide.
1) For room temperature
What is the range of room temperature? 25degC, 20 degC, or others? Another the room temperature may varies as time goes, will it affect the reslult(ID selection, GG)?
2) Voltage measurement
The fresh cell is connected to EVM (bq27541) with wire. There is some impedance of the wire. So when discharge the cell, there may be 5 - 10mV total lost. Will that affect the ID selection? And same to ra table?
3) System typical high discharge rate
May i use the 0.2C discharge rate as the system typical high rate(traditional optimization cycle)?
Best regards
J.C Chen