I am using BQ40Z60 IC in 3S1P Combination in my circuit. I have applied Adapter Voltage of 15V for Charging. But the Battery is not charging and also when I measure the Adapter Voltage Vac, its showing as 18.5V instead of 15V in Multimeter and in Battery Management Software. I am doubtful where to suspect whether in ACFET or HIDRV and LODRV.
ACFET gate pin showing 28V on Adapter Power and 0V without Adapter
HIDRV gate pin showing 11.8V on BOTH Adapter Power and with standalone Battery power (11.8V is the Battery Voltage at that time)
LODRV gate pin showing 0.4V on Adapter Power and 0.004V on Battery power respectively.
Kindly help on this issue with a solution