This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2400 lower OVP setting than 6.9V

Other Parts Discussed in Thread: TPS2400

Hi~

In TPS2400 OVP controller, OVP threshold is 6.9V, but customer want lower OVP setting level as 5.8V.

In application note, there are method to implement higher than 6.9V OVP but no under 6.9V OVP level.

Is there any method to implement 5.8V OVP threshold level in TPS2400?

If not, any good device for 5.8V OVP?

Thanks in advance.