Im working on a new circuit that involves a Li-io or Li-Po battery, typically a 18650 type (4.2V-2.7V) around 800mAh to 1600mAh.
To minimize the connectors on the circuit, i would like to use USB-Charging. So the maximum charging current would be 400mA
For the mcu and peripherals of the board, a sepic converter is needed to create 3.3V, 100mA with less than 50mV Ripple.
What Battery Charger is best for my application?
Is there a combined product that is a battery charger and integrated sepic converter?
If not, are there any recommend dc-dc sepic converters for use with batteries?