Hello team,
a customer of mine is using the TPS22860 with a battery at the output (Vout pin) and with the input that can switch between different state.
So I kindly ask you to provide more details about the behavior of the device when in output is present a battery.
Is there a reverse current protection?
If not, how is the behavior when in output there is a battery and on the ON pin there is 0V or 3.3V?
Thank you very much in advance for your support.
Best Regards,
Massimiliano De Cristofaro
Central Application Engineer – Power Management
EMEA Central Application Team
Texas Instruments Deutschland