Other Parts Discussed in Thread: BQSTUDIO, BQ34110
Hi,
Can I use BQ studio (v1.3.52) ' Start Log' option to generate the zip file to be used for Gauging Parameter Calculator. Can anyone list down the steps to be followed for a 48V Lead Acid battery pack.
Are the following steps valid for a lead acid battery pack also.I got the following steps from sluc138dj 'chemselect_cont.pdf' document.
1. Assemble a battery pack from a cell stack and EVM with a bq20zXX or
bq275xx battery gauging device. Thermistor must touch the battery cells, use
thermistor connections with flexible wires to do so!
2. Connect EV 2300 to the battery pack using SMB (or I2C, or HDQ connection
depending on the communication device uses )
3. Start EV Software
4. Start EV Software logging. Alternatively use external tester such as Arbin to log
time, voltage, current and temperature. Voltage must be measured with better than
1mV error.
5. Charge cell to the manufacturer specified voltage,
until taper current reaches C/100
6. Wait 2 hrs
7. Discharge at C/10 rate to manufacturer specified termination voltage
(use 3V if unknown)
8. Wait 5 hrs
9. Use chemselect_cont.mcd worksheet to find chemical ID (MathCad 11 or higher is
needed). After opening worksheet in mathcad, change column assignments for
t,V,I,T to match actual data-file column numbers.