We used TI BQ27421-G1A gauge in our product.
Currently, the golden image is only loaded into gauge when the battery had been disconnected.
1) After the plastic case of the product is put on the PCB Assembly, if the golden image is updated in F/W image,
it is necessary for the customer to disconnect the battery inside.
In order to reload the golden image into the gauge.
1-1) But this behavior is not REASONABLE and user-friendly.
2) If we reload the golden image into the gauge every time when gauge driver was initialized during the bot-up of system,
it will over-write the parameters in Data Memory of gauge every time when the system booted up.
2-1) Are there any side-effect if we do so?
Thank you.