Dear sirs,
For over a year now we are using UCC28600D in our power supply without any problem. But a week ago we encountered a problem. The voltage output, after thirty minutes, decays from 12,3V (normal value) to 11,0V. Analyzing with a scope, this voltage shows a ripple with 3 V peak-to-peak and a waveform like a sawtooth. For this case, power supply is only energized by AC power, without any load on this output.
Then, we note that replacing UCC28600D for another, output remains without any ripple and voltage doesn´t decays.
But, if we use a “type” of UCC28600D (event though it is a new part, picked up from the reel), the defective behavior remains. If the top mark of this part have a Texas logo filled, our power supply works without any problem. If this logo isn´t filled, we have this problem.
This test was realized in 10 boards. The defective behavior follows the chip with “not-filled” logo. We are thinking that this component may be counterfeit.
This part was supplied by an authorized distributor in Brazil (Arrow).
Is there someone here with any problem like this? Even if it´s with another part number. And, is there someone can say if two logo´s drawing are used by Texas Instruments?
Below, some photos with the two “types” of chip and another photo of this reel.
Best regards.
Valdecir