Hello
According to the data sheet the achievable dimming range is greater than 13000:1.
Is this range is available by using the PWM dimming only or is this is a combined dimming (including current dimming)?
Thanks
Valeri
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
According to the data sheet the achievable dimming range is greater than 13000:1.
Is this range is available by using the PWM dimming only or is this is a combined dimming (including current dimming)?
Thanks
Valeri
Hi Valeri,
13000:1 dimming ratio is achievable when using only PWM dimming, no need for current or hybrid dimming. Typically the limiting factor for dimming ratio is the LED driver rise time and LED PWM period. So we can estimate dimming ratio as Tp_LEDPWM / Tr_LEDRISE. For example, with a 100Hz PWM (10ms) and a 400ns rise time (typical value for LP8860 minimum on time PWM input) the dimming ratio will be 10ms / 400ns >13000:1.
Hope this helps.
Salome
Hi
Thanks for your help - this answers my question.
The problem that somehow I can't test the PWM pin input method on the EVM. I do can play with the PWM via the I2C registers. I did exactly what user guide of the EVM says, but the PWM pin control doesn't work - the LEDs stay OFF.
May be you know what can cause this problem?
Thanks
Valeri