This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560: compared to Ψjb=23.4℃/W, θjb=23.4℃/W and θJCtop=45.8℃/W

Part Number: TPS54560

Hi all

Would you mind if we ask TPS54560?

Ψjb=23.4℃/W and θjb=23.4℃/W are the same value.
However, compared to θJCtop=45.8℃/W, there is big difference about value.
So, why is there significant difference?

Kind regards,

Hirotaka Matsumoto