This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Lost communication with the chip after programming Golden Learning Image

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO

Hello everyone,

I am using custom board with a BQ34Z100-G1 on it. This chip runs well for several months but totally fails to connect after a successful image programming.

I tried following things.

  • Reprogram it but still no acknowledge from device
  • Execute FW but failed to execute Firmware - No acknowledge from device
  • Disconnect battery, reconnect to board and try steps above still the same result.
  • Directly issue I2C commands. I2C Command 0x00: Data block 0x000F I2C Command 0x64: Data block 0x000F I2C Command 0x65: Data block 0x0000

The REG25 output is stable and no ACK from I2C.

I am using the latest version of bqStudio (1.3.54) and EV2300's version is 3.1r. Any suggestion is welcomed.