Hello everyone,
I am using a custom board designed for measuring batteries remaining capacity. The batteries are charged with solar power, which is not stable, and discharged overnight. The load is wireless modules, typically 10mA during sleep and 300mA during active. After several day's monitoring, I find there are some jumps and drops of remaining capacity.
BQ34Z100-G1 is calibrated and runs well with a constant power supply and constant load.
Here is a log file. I plot the data so that you can see it clearly. Thanks.