Hi Team,
I have two question for the TPS65192.
On datasheet of TPS65192, it describes the 4 phase operation and 6 phase operation.
I am not sure the device will support 2 phase operation with GPM if signals sent to IN1, IN4 and FLK1 but IN2,IN3,IN5,IN6,FLK2 and FLK3 are grounded.
Can I get the output signal like figure1.
The other question is whether the TPS65192 allowed the 4 phase operation with GPM and without overlap of each phase like figure2.
(signal sent to IN1,IN2,IN4,IN5,FLK1,FLK2, Grounding with IN3,IN6 and FLK3.)
Figure1.
Figure2.