The data below is very typical for a particular battery pack in my space. The pack is being pulled by a Constant Current Load, But it is reproducible elsewhere in our space. The E-Load (sitting at ambient) has ~5mA of offset of its own, which is accounted for in this narrative. - Further, this parabolic trend (cenetered around room temp) appears at 3A as well. - For rated 0 to 50C range of operation, this data shows about 5% of spalsh. - At the high and low tempoeratures, there is a corresponding offset in the reading with 0 current pull. In other words, at 50C, there is about +50mA of current pull, evenb with no load on the battery. - This, whatever is drifting here, it appears to be an offset term What are the prime suspects for this phenomena?
I (-20C) = -927mA
I (0C) = -986mA I (15C) = -1004mA I (25C) = -1007mA I (50C) = -949mA Regards, Michael A. Banak