This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Isolated Flyback Controller with Coupled Inductor



Dear all,

does have TI an reference design for isolated DC/DC Flyback with coupled inductor like Colicraft LPR4012-223D ?

The wattage of the DC/DC less than 5W required ( approx 3.5W)

Best Regards. 

  • Can you specify more details for your spec and requirements?

    I.e. the input voltage min/max, output voltage and output max load power, target switching frequency, isolations requirements, etc?


    With more information, we will be able to make a better recommendation.

    Thanks,
    Bernard
  • Dear Bernard,

    I was interested on how to design a Flyback with coupled inductor and not with an Transformer . IS there an App note how do do this?

    Input voltage up to 57V if PoE is used, if not max input voltage 24V

    Consumption max 3.5W @ 5V output.

    As I saw the switching of an flyback controller is around 250kHz

    Best Regards.
  • Since a Flyback transformer is really a coupled inductor rather a conventional transformer, then yes, a Flyback power stage can be built around a coupled-inductor - if the 1:1 turns ratio is appropriate for the power stage, and if the pri-sec isolation of the coupled inductor is adequate for the application.

    It all depends on the input voltage range, output voltage, power level, etc.

    You can search all available TI-Designs and reference designs here:
    www.ti.com/.../refdesignsearchresults.tsp

    You can click on the "Search power design by parameters" tab, then enter your specs/requirements to refine the results to find the closest match.

    I hope this helps answer your question, if so, please click the "verify answer" button.

    Thanks,
    Bernard